Pipe Network Concept
In this figure, the mechanical system is composed of three-axes and driven by one motor.
- All axes are connected to the motor through shafts, gears and cams.
- When the motor is in motion, all axes are moving synchronously.
- The speed relation between the Master and the Axis is achieved by using a mechanical Gear.
- A mechanical cam is used to get linear motion from a rotating wheel.
The Pipe Network in this figure corresponds to the mechanical system described above.
The pipe concept is a one-to-one translation of a mechanical system into the logical world.
Figure 9-7: Pipe Network Structure
In our Pipe Network, the analogy is:
- The main motor of the mechanical machine becomes a Virtual Master Pipe Block.
- The gear boxes becomes Gear Blocks.
- The mechanical cam becomes a Cam Block.
- The axes becomes Axis Blocks.
The Pipe Network concept allows motion engineers to define, in a very natural way, the physical relationships between the different axes of their machine.
This modular approach provides a solution for almost any multi-axis requirements. It remains open for new, additional functions that can be required in the future.